Hi
Per Data sheet of HMC1081 mixer, 1dB Gain Comp input level +10dBm typ at Up conversion .
Also max rating RF input +3dBm??
Do you have any data for RF input 1dB comp? 60GHz is fine.
BR
Tatsu
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
HMC1081
Recommended for New Designs
The HMC1081 is a double balanced mixer. It can be used as an upconverter or a downconverter, with DC to 26 GHz at the IF port and 50 to 75 GHz at the RF...
Datasheet
HMC1081 on Analog.com
Hi
Per Data sheet of HMC1081 mixer, 1dB Gain Comp input level +10dBm typ at Up conversion .
Also max rating RF input +3dBm??
Do you have any data for RF input 1dB comp? 60GHz is fine.
BR
Tatsu
Hi Tatsu,
The IP1dB and Absolute Max states different things.
In the lab the part was pulsed to measure P1dB so that it is reliable.
The absolute max for the RF and IF for the part is determined by the max current handlings of the diode fingers, assuming an LO is applied as well. Above this absolute max power if a CW signal is applied for a long period the part might function but not be reliable in the long term. For higher RF/IF absolute power handling the LO Power needs to be reduced.
We do not have 1dB input compression data for downconversion.
Thanks,
Taz
Thank you Taz