Post Go back to editing

Using ADF4159 for a CW Radar application

Thread Summary

The user is developing a continuous radar system and inquired about disabling the 'Ramp On' function in the ADF4159 PLL to achieve a constant frequency. The final answer confirms that setting the 'Ramp On' bit to zero will lock the ADF5901 output to a constant frequency. The user also considered the ADF5902, which can similarly be configured for constant frequency operation. Additional advice was given on using ADIsimPLL for modeling and designing the loop filter to connect the charge pump to the V_Tune port.
AI Generated Content
Hi,

im studying electrical engineering at RWTH Aachen. Right now im doing my master thesis at the Chair of High Frequency Electronics.
For my thesis I'm going to develop a radar system which will be used for tracking purposes.
At the moment im trying to figure out what parts I'm going to need for my application.
While researching, I stumbled upon the ADF4159(https://www.analog.com/en/products/adf4159.html), which I want to use as a PLL for my frequency synthesis (the PLL will be used in combination with the ADF5901). As im going to develop a continuous radar, my main goal with this PLL is to operate it at a costant frequency. While studying the datasheet, I was able to spot that there is a register (DB31; p.15) for using/disabling a "Ramp On"-function.
So here is my question: If i set the "Ramp On"-Bit to zero, will the PLL operate at a constant frequency instead of functioning as a FMCW?
And if thats not the case, could you recommend a different PLL for my desired purpose? I would be absolutely grateful if you could enlighten me on this matter. Thanks in advance! Sincerely yours Niklas
Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.