Post Go back to editing

Applying voltage to INPT terminal of ADL5303

Hi,


We are considering a circuit configration as shown in the figure below.


When switching between passing the current mirror (ADL5315) and not passing the current mirror with the analog switch (ADG783),
a voltage (= ADG783's on-resistance x IPD) is applied at the INPT pin of ADL5303.
Does this voltage affect the accuracy of IPD monitor on the ADL5303?

Regards,

Hase

Parents
  • Greetings Hase,

    ADL5303 input voltage is determined by the voltage on it's VSUM pin. Looking at the ADL5303 block diagram (datasheet page 1), we see the NPN logging transistor is driven such that the voltages on the two op-amp inputs are held equal.

    Applied to this application, it means the voltage at INPT holds relatively constant, while the voltage on the other side of the ADG783 switches is what should go up according to IR drop. The DAC output may need higher output voltage setting for higher Ipd current.

    -Bruce H.

Reply
  • Greetings Hase,

    ADL5303 input voltage is determined by the voltage on it's VSUM pin. Looking at the ADL5303 block diagram (datasheet page 1), we see the NPN logging transistor is driven such that the voltages on the two op-amp inputs are held equal.

    Applied to this application, it means the voltage at INPT holds relatively constant, while the voltage on the other side of the ADG783 switches is what should go up according to IR drop. The DAC output may need higher output voltage setting for higher Ipd current.

    -Bruce H.

Children