Post Go back to editing

EVAL-HMC1023LP5 and HMC6356 USB Interface

Thread Summary

The user had issues with the EVAL-HMC1023LP5 and HMC6356 USB interface card using the DLP2232H. The correct jumper settings are JP1 short and JP2/JP3 open. The user also needed to install specific DLP2232H USB drivers and add a 10pF cap in parallel with R55 to resolve communication issues.
AI Generated Content

I have a EVAL-HMC1023LP5 and driving it with a HMC6356 USB interface card. This interface card appears slightly different them the one shown in the the photos 

The usb interface card is using DLP2232H. https://www.dlpdesign.com/dlp2232h-ds-v11.pdf. 

There does not appear to be a SPI output coming from this output header. Do you have a schematic for the HMC6356?

Chris

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.