Post Go back to editing

EVAL-HMC1023LP5 and HMC6356 USB Interface

Thread Summary

The user had issues with the EVAL-HMC1023LP5 and HMC6356 USB interface card using the DLP2232H. The correct jumper settings are JP1 short and JP2/JP3 open. The user also needed to install specific DLP2232H USB drivers and add a 10pF cap in parallel with R55 to resolve communication issues.
AI Generated Content

I have a EVAL-HMC1023LP5 and driving it with a HMC6356 USB interface card. This interface card appears slightly different them the one shown in the the photos 

The usb interface card is using DLP2232H. https://www.dlpdesign.com/dlp2232h-ds-v11.pdf

There does not appear to be a SPI output coming from this output header. Do you have a schematic for the HMC6356?

Chris

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.