ADF4356: Phase Adjust in Integer-N mode

Hi,

we are trying to use the phase adjustment function of the ADF4356 in Integer-N mode. We tried to force the SD-Modulator to run in Integer-N mode as described here for the ADF4355: https://ez.analog.com/rf/f/q-a/110417/4355-2-phase-adjust-integer-n/333601#333601

However, after setting Muxout to "Reserved" and SD Testmodes to "0100 - SD EN with FRAC = 0" the output signal disappears and is only briefly visible while executing the Init Sequence or Frequency Update Sequence. Interestingly, when updating only R3 or R7, the signal reappears and when updating R0 or R4 it disappears again. But even when the signal is present, the phase adjustment is still not working in Integer-N mode.

Can you please confirm that this method works with the ADF4356 at all?

Best regards,
Thomas