ADF4371 with HMC1031/ADF4002, 20dB Phase Noise hit at 100Hz Foffset

Hi ADI,

I have an eval for the ADF4371 and I'm using an HMC1031 eval to lock the 100MHz ref to a precision 10MHz OCXO.  I am generating an 18GHz LO.  As seen here:

The problem here is measured PN at 100Hz offset.  With the on-board crystal reference PN @ 100Hz = -87dBc/Hz.  With HMC1031 PN @ 100Hz = -67dBc/Hz.

Notable design parameters:

- HMC1031 Loop BW set to 10Hz as outlined in the spec sheet page 12.  www.analog.com/.../hmc1031.pdf

- 100MHz VCXO, CVHD-950, CMOS output

- The measure slew rate from the HMC1031/CVHD-950 better than on board 100MHz reference.

Thanks in advance!

Chris



Added other parts to title
[edited by: aandrews at 4:14 PM (GMT -4) on 24 Sep 2021]
Parents
  • Hi Chris,

    The Flicker FOM of HMC1031 is -252dBc/Hz. This gives -112dBc/Hz @ 100Hz offset @ 100MHz output.
    PNFLICK = Flicker FOM + 20log(fVCXO) − 10log(fOFFSET)

    If this is transferred to 18GHz;
    -112 -20log(18G/100M) = -67dBc/Hz.

    If I did not make any mistake in calculations, math says that your measurement is very accurate. The contributions from other sources (OCXO, VCXO, PLL floor FOM, loop filter) are not significant.

    When using CVHD in open loop, I would also expect to see something close to -87dBc/Hz. But it is possible that the instrument cannot track the signal as you advised. Perhaps you can try to force Vtune to a mid-level instead of connecting it to GND. Min and max levels might be problematic.

    Regards,
    Kazim

  • Hi Kazim,

    So based on the recommendations here:

    https://ez.analog.com/clock_and_timing/f/q-a/167636/easy-to-use-jitter-attenuator-reference-cleanup-loop-examples/379866#379866

    It looks like the ADF4002 would be a good fit to improve my phase noise performance by an additional 7dB based on the improved 1/f FOM of -259dBc/Hz of the ADF4002 vs. -252dBc/Hz for the HMC1031.

    However, I am not able to realize the performance suggested by the ADF4002 model in ADIsimPLL.  I am seeing generally the same performance with both the ADF4002 and the HMC1031.  I've been through a couple iterations on the loop filter and have double checked the setting in the Integer N software.  So I'm kind of stuck, any suggestions?

    Regards,

    Chris

Reply Children
  • Hi Chris,

    Is it possible that you are around the measurement limits of your signal source analyzer? 

    Kudret

  • Hi Kudret,

    For the ADF4002 or the HMC1031 at 100MHz yes.  But at 18GHz output from the ADF4371 is definitely in the measurement range.  Switching between the 4002 and the 1031 as reference for the ADF4371 PN performance is degraded using the 4002 at all offsets.

    Regards,

    Chris

  • Hi Chris,

    HMC1031 is dominating element for the 100Hz PN.

    When using ADF4002, it is possible that OCXO, VCXO and other elements are also contributing. CVHD-950 datasheet typical spec is -119dBc/Hz at 100Hz offset for 100MHz output. Can you please check the PN of OCXO? Did you model these components in ADIsimPLL when simulating your circuit?

    At these low levels supply noise may also affect the measurements.How do you power the ADF4002 and CVHD-950, are you using LDOs? Can you check with different bench power supplies? Is it possible to share the screenshot of your measurements?

    Regards, Kazim

  • Hi Kazim,

    I do not have an instrument that can measure PN of an OCXO.  So I rely on the measurements at RF to imply the PN at the reference frequency.

    I did model the 4002 in ADIsimPLL I can share if you would like to see it.  The SW shows -118dBc/Hz at 100Hz offset.  This would imply -72dBc/Hz at 18GHz.  This is acceptable if I could realize it.

    I am powering the ADF4002 eval unit from bench supplies.  I will try some other supplies and see if there is any improvements seen.  I will also share some screenshots of the measurements soon.

    Regards,

    Chris

  • Hi Kazim,

    As seen below I was able to realize some improvement in PN performance of the ADF4002 by reducing power supply noise.  PN measured at 18GHz.

    PN plot:

    However, by implementing similar changes to the 1031 circuit I was able to improve the performance of that as well and it still outperforms the 4002.