Hello Sir/ Maam,
I am looking for a mixer eval board that can be useful for phase measurement of RF and LO. The expected output at I and Q is DC single ended signal since both the input freq is same. I and Q output of IF may be used for phase measurement. Ports at 50 ohm impedance and single-ended. We had already purchased ADL5380 eval board but due to its differential output and required soldering to change the configuration to single-ended and output of the same could only be observed on the load resistor and not on the output port that we have dropped the board which has even got damaged in the process to make the configuration settings.