Post Go back to editing

Single ended operation in ADL5380 for DC output

We have the eval board of ADL5380. We desire to operate it in a single-ended mode. As suggested in the datasheet the RF and LO input already has a 100pf capacitor connected to one port and ground on the eval board for single-ended mode.  According to the datasheet per pin impedance is 25ohm so in the eval board with the onboard baluns connected do we need to match it at 50ohm since according to the datasheet all the pins are at 25ohm impedance or all are at 50ohm differential. Please correct if any confusion in understanding. 

We have given 5.81Ghz input to RF port at -10dBm and 5.81Ghz input to LO at -5dBm. The board I guess is by default configured to single-ended operation since the SMA connecter not connected to RFIN & LOIN and 100pf already connected. ILO & QLO we have terminated with 50ohm. Is the experiment setup correct or we have to make changes to work in a single-ended configuration? 

We expect a DC signal at the output I and Q single-ended but while observing on the scope but we find the noise at 10mV. We want to observe a DC signal flat line and only the phase difference between the RF and LO. Please correct us if any mistakes and suggest a way to achieve the same. Attaching images of the test setup and observations on the scope for 5.81Ghz at the RF and LO. Using this setup we have also done a trial with 4.7Ghz and 4.8Ghz at the RF and LO respectively to and we could observe 100Mhz signal at around 160mV as shown in the attached image.

    

Parents
  • Hi akshay92,

    • Attached is the latest version of the schematic for the board which you have in the photo.
    • To help troubleshoot, please markup the schematic and send back with any changes you have made.
    • Be sure the RF and LO sources are synchronized or there could be residual frequency error due to the internal references of each source. The residual error could cause an AC signal at the baseband outputs.
    • To measure true DC you will need to bypass the transformers on the baseband outputs, since the transformers will block DC.
    • The baseband differential load impedance should be kept above 200 ohms.
    • When connected with the baseband transformers and terminated into 50 ohms single ended, the differential load impedance presented to the device is 450 ohms.

    PDF

    Best Regards,

    David

  • Thank you for the timely response. We have gone through the updated schematic and I think it is the same what we have and we have not connected or removed any component.

    We are giving trigger to RF and LO at the same time, if there is any other way to make sure if signals are in sync then please guide for the same.

    From datasheet page number 34, table 5 it is shown that for the single-ended output, the resistors R2x-R5x needs to be populated for bypassing the output transformer and R13x-R18x needs to be populated for a single-ended mode. Please correct us if anything is written is incorrect. According to our understanding we have to populate registers at R2x-R5x.

    Another point which is not clear is about the 200ohm impedance, is the eval board configured for 50ohm per pin? please elaborate a little on this. And I guess since the output being DC we might not require any matching at the output ports, please correct if any mistake in understanding.

  • Hi akshay92,

    • We don't have measurements for your test conditions, but attached is data which was collected on a similar device the ADL5382, at 700 and 1000MHz. You could use the same test methodology for your evaluation.
    • We used an oscilloscope to measure phase and two DMM's to measure voltage across the load resistors. The more accurately you measure these two quantities, the more precise estimation of phase between the two paths.
    • The 2.4V you measured at the baseband outputs is the common mode voltage. Once you add the differential load resistor, you should see the voltages change as current flows through the resistor.
    • You could use an instrumentation amplifier or ADC driver as a buffer to convert the differential voltage across the resistor to a single ended voltage. This has the benefit of adjusting the voltage range and common mode voltage to in line with the next stage in your system (ADC, etc).

    XLSX

    Best Regards,

    David

  • Thank you for the response. Will do as you have suggested and get back as soon as possible.

  • Hello Sir,

    As you recommended above, for DC output we have to bypass the balun and add load resistor but before doing that we thought to test the output between  IC pin 3 and 4 and pin 15 and 16 directly through Multimeter.

    We just added Load resistor of value 500 ohm at R6x and R7x.

    So at LO/RF Freq 5.81Ghz and input power 0dbm , We were getting only 770 microV across R6x and for phase difference we changed the length of cable at RF side. so the voltage variation observed was from 500 microV to 1.4mV. 

    Is it right what ever we did? or need to Bypass the balun first and then carry out the experiment.  

    So can you help us with what exact value of the Load Resistor should be and what is the expected result range and please correct us if any mistake we have done.

  • Hi akshay92,

    • You will need to use the phase sweeping capability of the two RF sources, which are synchronized. Many sources will allow you to sweep the output phase. If the sources do not have that feature, you could use a mechanical phase shifter to sweep through various phase states.
    • Also, one additional change you may need is the leave the ADJ resistor open on pin 19. For operation above 5GHz, this will optimize the mixer configuration.

    Best Regards,

    David

  • Thank you so much sir. I’ll do the changes as suggested and get back to you if i face any problem.

  • We are able to see the output on the 500-ohm load connected at the I and Q port after making the resistor changes as suggested by you. We are able to see the change in the DC level when observed on the load resistor but when observed on the single-ended connector positive of I and Q we see a non-changing DC level of 2.4V or around 3V. Please guide on what else changes we have to make to see the output on the single-ended connector.

    After 2 days of testing, we are unable to see repetitive results as mentioned above. And no change in results after removing the resistor19. We now see a constant DC even at the load resistors of 500ohm. The current is same, means no damage to the board

  • Hi akshay92,

    The importance is the DC voltage across the load resistor. As the phase changes it causes the output stage to pump current from one side of the diff pair to the other.

    If you are working with Ankita, please let's use the other forum thread, so there is not information in two places.

    https://ez.analog.com/rf/f/q-a/535486/adl5380

    Thanks,

    David

  • Yes david ji, you guessed it correct. Working with Ankita. Actually due to current situation only one of us cud work in lab at a time so how to communicate in my absence, she made another thread. Sorry for the confusion. Further discussion we shall have it on other thread. Thank you for the response.

  • Hi akshay92,

    Ok, thank you. No worries, I just thought it would be easier to follow for all three of us if it was on one thread.

    Thanks,

    David

Reply Children
No Data