Post Go back to editing

about Evaluation board for ADF4360-9

Hi,

I have some questions about the evaluation board for ADF4360-9.

1. In the below user guide, Figure 1 and Figure 2 show a different version. the one is Rev.A, the other is Rev.E, I think Rev.E is the latest version, am I correct?

    https://www.analog.com/media/en/technical-documentation/user-guides/UG-106.pdf

2. Is the schematic in the user guide for Rev.A? 

     because there is a comparator connected to 20pin on the schematic, but it looks like no comparator on the Rev.E board( Figure 1).

     and if need a comparator, when should I use this option?

 

Best Regards,

Leo

Parents Reply Children