ADL5304 can detect 0.1pA current signal or not?Form the picture ,we can calculate that when current is 0.1 pA, and the Vlog about 0.2~0.3V? It's right or not。thanks !
ADL5304
Recommended for New Designs
The ADL5304 is a high speed logarithmic converter with fast response and low noise over a 200 dB (1 pA to 10 mA) measurement range. The ADL5304 provides...
Datasheet
ADL5304 on Analog.com

ADL5304 can detect 0.1pA current signal or not?Form the picture ,we can calculate that when current is 0.1 pA, and the Vlog about 0.2~0.3V? It's right or not。thanks !
Hi there,
It depends on the part, and temperature. Down at the low end of input current range, there will be more temperature variation:

If mass production application, see also datasheet Figures 11 and 13, and compare that against your accuracy requirement.
-Bruce H
Hi Bruce:
When VNEG is -5V, the mark trace is GND or not?the PCB layout show as fig2 is ok or not?
Thank you!
fig1:

fig2:

Hi there,
In Figure 1, the arrows point to copper that connects to the VSMx pins.
In Figure 2, we recommend a defined guard ring around the INUM node connections. Ref. datasheet page 26.
-Bruce
Hi Bruce: when use nea
Hi Bruce:
when use negative power, VSMx are connect to GND, so the Guard ring of INUM is GND or not?
Do you have the layout guide of Guard ring, like the Schematic diagram?
Hi Bruce:
when use negative power, VSMx are connect to GND, so the Guard ring of INUM is GND or not?
Do you have the layout guide of Guard ring, like the Schematic diagram?
You're correct. When VSMx= Gnd, the guard ring can also be Ground.