Hi,
Is it possible to use TinyRad outside of 24-24.250GHz frequency range? What I mean is to keep the bandwidth the same (250MHz), but shift it in the frequency domain (e.g. 23.750 to 24GHz). I did a quick test with a spectrum analyzer and MATLAB scripts and it looks like the radar is transmitting fine in other frequency ranges, however, I'm not sure if the data is reliable.
Thanks
Yes it is possible to use the TinyRad outside of the intended 250MHz ISM band at 24 - 24.25GHz by configuring the ADF4159, and there is some margin in the ADF5901's vtune to operate approximately…