Q: What are the individual stage currents for the four stages of the HMC943APM5E?
Q: What are the individual stage currents for the four stages of the HMC943APM5E?
A: For a bias current setting of 1300 mA which is the datasheet default, below are the individual stage currents.
Stage 1 top side (VD1): 43 mA
Stage 1 bottom side (VD2): 43 mA
Stage 2 top side (VD3): 87 mA
Stage 2 bottom side (VD4): 87 mA
Stage 3 top side (VD5): 173 mA
Stage 3 bottom side (VD6): 173 mA
Stage 4 top side (VD7): 347 mA
Stage 4 bottom side (VD8): 347 mA