Post Go back to editing

ADL5513 noise <1kHz

Thread Summary

The user is seeking data on the ADL5513's output noise density below 1kHz for a detector with an envelope bandwidth of 0-100Hz. The final answer suggests that the 1/f noise in the graphs may be influenced by the test setup, and the user measures a standard deviation of 0.002dB (42uV rms) at 100Hz, with a noise density of 4.2uVrms/sqrt(Hz). The user notes that increasing the acquisition bandwidth to 1kHz does not significantly increase the rms noise, indicating low-frequency noise dominance.
AI Generated Content

Hello, I'm using the ADL5513 for a detector with low envelope bandwidth, around 0-100Hz. The ADL5513 datasheet only describes output noise density down to 1KHz. Do you have any data below 1KHz for estimating output noise? The plots show it decreasing at around 20dB/decade, but I'm assuming it must flatten out at some point...

Regards,

Mike

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.