PLL ADF5610 Phase Noise query

Hi,

In ADF5610 PLL datasheet phase noise graph showing -104dBc/Hz at 10kHz offset for output freq 14.4GHz but in marker same data was measured as -107dBc/Hz.

So I simulated it using ADISIMPLL tool, here it was showing -99dBc/Hz for 14.4GHz at 10KHz offset. I attached simulation file also.

Kindly clarify which one is correct.

Parents
  • +1
    •  Analog Employees 
    on Jul 20, 2020 12:41 PM 7 months ago in reply to Pathu

    Hi,

    The phase noise plot in the datasheet is correct but the values in markers are not. Attached is the original measurement result at 14.4 GHz in which Wenzel OCXO is used as reference. I also attached measurements for 14.4 GHz and 8 GHz in which SMA100B is used as reference. Loop filter is same for all cases and it is also attached. 

    These references have very good phase noise and the ADISIMPLL results may not show such results if the reference is not good enough but it is the correct way to model your reference clock and to use that one in the ADISIMPLL simulation to get results similar with the actual design.

    Regards,

     Original Measurement

     SMA100B Measurement

     SMA100B Measurement

    Kudret

  • We have tested your ADF5610 eval-board using external low phase noise OCXO and observe similar phase noise for Integer mode.

    Whereas when we test using frcational mode like frequencies 13.45GHz, 14.41GHz then output spectrum also looks have more spurious and Phase noise is degraded by around 10dBc at 1, 10 & 100KHz Offsets.

    Can you please check in your test setup and provide phase noise plots like fractional output frequencies 13.45, 14.41GHz using 100MHz Wenzel OCXO?

Reply
  • We have tested your ADF5610 eval-board using external low phase noise OCXO and observe similar phase noise for Integer mode.

    Whereas when we test using frcational mode like frequencies 13.45GHz, 14.41GHz then output spectrum also looks have more spurious and Phase noise is degraded by around 10dBc at 1, 10 & 100KHz Offsets.

    Can you please check in your test setup and provide phase noise plots like fractional output frequencies 13.45, 14.41GHz using 100MHz Wenzel OCXO?

Children
No Data