Post Go back to editing

Residual phase noise of HMC575 and HMC573

The datasheets of the HMC575 and HMC573 frequency doublers only give residual phase noise at 100 kHz offset. Can you perhaps provide a graph over a wider offset frequency range?

Thanks.

Parents
  • Admittedly this should be easier to answer than it is.  I have not been able to find the original characterization data.  I was able to determine the number in the HMC575 datasheet was based on 4GHz input frequency.  From there you can mathematically determine some reasonable numbers using these formulas.

    100kHz PN = datasheet number + 10*log(fout/4GHz)

    For different phase offset you can use a 10*log(offset frequency) curve.

    What particular frequencies and offset are you interested in?  

Reply
  • Admittedly this should be easier to answer than it is.  I have not been able to find the original characterization data.  I was able to determine the number in the HMC575 datasheet was based on 4GHz input frequency.  From there you can mathematically determine some reasonable numbers using these formulas.

    100kHz PN = datasheet number + 10*log(fout/4GHz)

    For different phase offset you can use a 10*log(offset frequency) curve.

    What particular frequencies and offset are you interested in?  

Children