Post Go back to editing

FAQ: HMC936A Operation Below 1.2 GHz

Thread Summary

The user inquires about operating the HMC936A phase shifter below its specified frequency range. The support engineer explains that this is challenging due to insufficient electrical length and suggests the ADL5390 as an alternative for lower frequencies (20 MHz-2.4 GHz), noting it requires an external 90° phase splitter and can be configured with I and Q control voltages. For digital phase shifting, additional DACs are necessary.
AI Generated Content
  • A: Operating phase shifters outside of their specified frequency range, particularly at the low frequency end, is difficult because you run out of electrical length. 

    An option for phase shifter of lower frequency range is ADL5390, that can be used as wideband vector modulator (20 MHz-2.4 GHz). It does require an external 90 deg phase splitter to be made operational. Also, the phase is controlled by two analog voltages, an I control voltage and a Q control voltage. If digital phase shifter is needed, additional two DACs are required.