Dear Sir,
As enclosed measured on EVB, the gain difference between specification on datasheet & S parameter "ADPA7005AEHZ.s2p" on web. Would you kind to released de-embedded S2P for clarification on this ? Thanks.
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
ADPA7005
Recommended for New Designs
ADPA7005AEHZ
The ADPA7005 is a gallium arsenide (GaAs), pseudomorphic high electron mobility transfer (pHEMT), monolithic microwave integrated circuit...
Datasheet
ADPA7005 on Analog.com
Dear Sir,
As enclosed measured on EVB, the gain difference between specification on datasheet & S parameter "ADPA7005AEHZ.s2p" on web. Would you kind to released de-embedded S2P for clarification on this ? Thanks.
Hi Kenton,
Figure 10 in the data sheet is measured with a -20 dBm input signal. Could you perform a full 2 port calibration at -20 dBm? I want to confirm the small signal results match Figure 10 from the data sheet. I want to determine if there is a measurement issue or a device issue.
Regards,
Jim B
Jim,
Glad to have your input. Actually, the result is same as -20dBm input shown above. If any ignored, be free to inform.
Thanks
Hi Kenton,
I assume you are using the E3634A power supply for the drains. Am I correct? Are you using remote sense? If not you should be remote sensing the drain voltage. I think you might have a voltage drop and 5 V is not at the device pins. Can you bias the amp and measure the drain voltage at the pins? It should be 5 V.
Regards,
Jim B
Hi Kenton,
I assume you are using the E3634A power supply for the drains. Am I correct? Are you using remote sense? If not you should be remote sensing the drain voltage. I think you might have a voltage drop and 5 V is not at the device pins. Can you bias the amp and measure the drain voltage at the pins? It should be 5 V.
Regards,
Jim B
Jim,
We're using power supply E3631A and pin voltage is 4.8V, read by portablemeter U1252B.
Try to lift pin voltage to 5V abd result as below screenshot.


Hi Kenton,
Yes, That looks much better. I'm trying to attach the thru data but I'm unable to at this time. I will upload when the system is fixed.
You can down load the S-Parameter files from the link below. The thru data file is in the zip folder. You can the subtract S21 thru from the S21 magnitude of your data and you will be very close to what is shown in the data sheet.
https://www.analog.com/media/en/simulation-models/s-parameters/ADPA7005AEHZ.zip
I measured the ADPA7005AEHZ s2p file, displayed the data with the same scaling you are using and the data lined up rather nicely.
Regards,
Jim B
Jim,
Thanks. The problem has fixed.