LTC6431-20
Recommended for New Designs
The LTC6431-20 is a gain block amplifier exhibiting excellent linearity at frequencies beyond 1000MHz and with low associated output noise.
The unique...
Datasheet
LTC6431-20 on Analog.com
Hi,
I would like to confirm S-parameter files provided for LTC6431-20 are correct. I see mention of port 3 in the header which does not make sense to me for this amplifier, and I also notice the data goes up to 5GHz which is well beyond the rated operation for the part which makes me think something is not correct. I am not sure what "SOLT2" in the header refers to either.
Can someone please confirm if the S-parameter file linked below is correct, or if not provide correct S-parameter file?
I am referencing S-parameter file here:
https://www.analog.com/en/products/ltc6431-20.html
https://www.analog.com/media/en/simulation-models/s-parameters/LTC6431_20_SPARs_25C.S2P
Below is what I see in header of file.
!Agilent Technologies,E5071C,MY46100626,A.10.05
!Date: Tue Dec 10 16:09:51 2013
!Data & Calibration Information:
!Freq S11:SOLT2(ON) S31:SOLT2(ON) S13:SOLT2(ON) S33:SOLT2(ON)
Thanks,
Steve