LTC6431-20
Recommended for New Designs
The LTC6431-20 is a gain block amplifier exhibiting excellent linearity at frequencies beyond 1000MHz and with low associated output noise.
The unique...
Datasheet
LTC6431-20 on Analog.com
Hi,
I would like to confirm S-parameter files provided for LTC6431-20 are correct. I see mention of port 3 in the header which does not make sense to me for this amplifier, and I also notice the data goes up to 5GHz which is well beyond the rated operation for the part which makes me think something is not correct. I am not sure what "SOLT2" in the header refers to either.
Can someone please confirm if the S-parameter file linked below is correct, or if not provide correct S-parameter file?
I am referencing S-parameter file here:
https://www.analog.com/en/products/ltc6431-20.html
https://www.analog.com/media/en/simulation-models/s-parameters/LTC6431_20_SPARs_25C.S2P
Below is what I see in header of file.
!Agilent Technologies,E5071C,MY46100626,A.10.05
!Date: Tue Dec 10 16:09:51 2013
!Data & Calibration Information:
!Freq S11:SOLT2(ON) S31:SOLT2(ON) S13:SOLT2(ON) S33:SOLT2(ON)
Thanks,
Steve
Moved to the amplifier forum
Moved to the amplifier forum
Hi lithelycanthrope,
SOLT stands for Short, Open, Load, Thru calibration.
The measurement may have been taken up to 5GHz to make sure there is a clean spectrum even beyond the part's operational range.
Port 3 seems to be just a substitute for Port 2 (which is missing). I'll confirm with the Product Line and let you know if there is any discrepancy in the S-parameter model of the LTC6431-20.
Regards,
Hooman