KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
LTC6431-20
Recommended for New Designs
The LTC6431-20 is a gain block amplifier exhibiting excellent linearity at frequencies beyond 1000MHz and with low associated output noise.
The unique...
Datasheet
LTC6431-20 on Analog.com
Hi,
I would like to confirm S-parameter files provided for LTC6431-20 are correct. I see mention of port 3 in the header which does not make sense to me for this amplifier, and I also notice the data goes up to 5GHz which is well beyond the rated operation for the part which makes me think something is not correct. I am not sure what "SOLT2" in the header refers to either.
Can someone please confirm if the S-parameter file linked below is correct, or if not provide correct S-parameter file?
I am referencing S-parameter file here:
https://www.analog.com/en/products/ltc6431-20.html
https://www.analog.com/media/en/simulation-models/s-parameters/LTC6431_20_SPARs_25C.S2P
Below is what I see in header of file.
!Agilent Technologies,E5071C,MY46100626,A.10.05
!Date: Tue Dec 10 16:09:51 2013
!Data & Calibration Information:
!Freq S11:SOLT2(ON) S31:SOLT2(ON) S13:SOLT2(ON) S33:SOLT2(ON)
Thanks,
Steve
Moved to the amplifier forum
Hi lithelycanthrope,
SOLT stands for Short, Open, Load, Thru calibration.
The measurement may have been taken up to 5GHz to make sure there is a clean spectrum even beyond the part's operational range.
Port 3 seems to be just a substitute for Port 2 (which is missing). I'll confirm with the Product Line and let you know if there is any discrepancy in the S-parameter model of the LTC6431-20.
Regards,
Hooman
Hi Steve,
The S Param file does show PORTs 1 and 3. It is still a 2 Port measurement. We have a 4 port network analyzer and just used Port 1 and 3 to make a 2 Port measurement. We show the results far beyond the intended operational range. This is to show that the parts are stable and not oscillating out there. With modern transistors the Ft can be over 50GHz and FMAX of 80GHz it is very important to amke sure the devices are behaving even outside of your intended band. If a device is oscillating outside your band it will still hammer the linearity in band. Few other manufacturers provide this level of info but it is very important.
The measurements are based on a SOLT calibration as Hooman has outlined. The measurements are referenced to the package pins.
Regards,
Greg Fung
Hi Steve,
The S Param file does show PORTs 1 and 3. It is still a 2 Port measurement. We have a 4 port network analyzer and just used Ports 1 and 3 to make a 2 Port measurement. We show the results far beyond the intended operational range. This is to show that the parts are stable and not oscillating out there. With modern transistors the Ft can be over 50GHz and FMAX of 80GHz it is very important to make sure the devices are behaving even outside of your intended band. If a device is oscillating outside your intended band it will still hammer the linearity in band. Few other manufacturers provide this level of info but it is very important.
The SPARM measurements are based on a SOLT calibration as Hooman has outlined. The measurements are referenced to the package pins.
Regards,
Greg Fung
Thank you very much for the info and for the verification!