Post Go back to editing

SysParameters

Thread Summary

The user inquired about obtaining more accurate IP2 data for HMC636 and HMC374, both with a P1dB of 22 dBm. The support engineer confirmed that IP2 data was not measured for these parts, and the GaAs devices' consistency in P1dB/IP2 offset was used instead. The user also sought help with converting a SysParameter model from Genesys to ADS, and the support engineer provided a correctly structured MDF file example, which resolved the issue.
AI Generated Content

Hi,

I noticed that the IP2 parameter is usually entered as 20dB above P1dB.  Is there any way to get more accurate IP2 data?

I am specifically wanting to know which part has better IP2 performance, HMC636 or HMC374.  Both have P1dB = 22dBm.

Regards,

Chris