Post Go back to editing

rise time of power amplifiers: HMC8500PM5E and HMC1099PM5E

Hi, I am looking for a power amplifier for pulsed operation at 300MHz RF carrier.

I need to know the rise time of the folowwing models: HMC8500PM5E and HMC1099PM5E

do you have this parmater measured?

or can I use LTSPICE or ADS simulation to measure it?

thank you

Parents Reply Children
  • hi,

    thank you, but this measurment gives no info:

    first note that rise time is defined of time to reach 10% to 90% of amplitude. 10% means -20dB, so I think you can measure the time from -20dBc to full power (~10msec)

    second, note that VBW in the meauisrmnet is 91Hz. which means it slows the rise time by the spectrum analyzer itsekf. so rise time is ~1/91Hz = ~ 10msec

    the correct way to measure is increasing VBW to hundreds oh MHz (because I expect rise time is order of 10nsec). or use osciloscope with suffucuent analog BW (300MHz rf carrier is enough for me)

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.