Can you provide a schematic diagram of the EVAL-HMC920LP5E board? The PADS PCB layout file is provided in the "HMC920LP5E Full Gerber Files" ZIP file, but a schematic diagram in PDF form would be helpful as well.
Can you provide a schematic diagram of the EVAL-HMC920LP5E board? The PADS PCB layout file is provided in the "HMC920LP5E Full Gerber Files" ZIP file, but a schematic diagram in PDF form would be helpful as well.
Hi Ivan,
Please send the schematic to me as well.
Thanks
,
Bill
Thanks.
I plan to use the 130511-HMC920LP5E evaluation board with the 117494-HMC659LC5 eval board. Given Idrain is 300 mA for the HMC659LC5, using equation 4 in the data sheet, Rsense calculates to be 576 ohms. I assume I need to short R4 and adjust R19 to 576 ohms?
Thanks.
I plan to use the 130511-HMC920LP5E evaluation board with the 117494-HMC659LC5 eval board. Given Idrain is 300 mA for the HMC659LC5, using equation 4 in the data sheet, Rsense calculates to be 576 ohms. I assume I need to short R4 and adjust R19 to 576 ohms?
Sorry, I don't know the answer to that. It's best to start a new query so that the HMC920 applications engineer will be tagged and can answer the question.