Q: Can you provide Residual Phase Noise Data for HMC566LP4E?
HMC566LP4E
Production
The HMC566LP4E is a high dynamic range GaAs pHEMT MMIC Low Noise Amplifier (LNA) in a 4x4 mm SMT package which operates from 28 to 36 GHz. The HMC566LP4E...
Datasheet
HMC566LP4E on Analog.com
Q: Can you provide Residual Phase Noise Data for HMC566LP4E?
A:
Figure 1 shows the residual phase noise of HMC566LP4E, measured at an output power of 14 dBm (PSAT, PIN = -5 dBm) at 30 GHz. Figure 2 shows the baseline phase noise of the measurement setup.

Figure 1. HMC566LP4E Residual Phase Noise, POUT = 14 dBm (PSAT, PIN = -5 dBm) at 30 GHz

Figure 2. Baseline phase noise of measurement setup
* VDD = 3 V, IDD = 82 mA