Post Go back to editing

FAQ: Residual Phase Noise of HMC383LC4

Q: Can you provide Residual Phase Noise Data for HMC383LC4?

  • A:

    Figure 1 shows the residual phase noise of HMC383LC4, measured at an output power of 16 dBm (P1dB, PIN = 0 dBm) at 25 GHz. Figure 2 shows the baseline phase noise of the measurement setup.

    16 dBm (P1dB, PIN = 0 dBm)

    Figure 1. HMC383LC4 Residual Phase Noise, Pout = 16 dBm (P1dB, PIN = 0 dBm) at 25 GHz.

    Figure 2. Baseline phase noise of measurement setup.

    * VDD = 5 V, IDD = 100 mA

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.