Post Go back to editing

HMC1055

Friends,

Intendto use HMC1055 for protection application with 2860 MHz.

Please clarify RF1 (as OUT), and RF2 (as IN) are interchangeable?

I intend to provide the RF2 port with internal termination, to which RF signal generator is connected.

Kindly note: Figure 1 of internal diagram and page 8 of Data sheet explanation are contradictory. Pls write which one is true.

Thanks 

Venkataramanan

Parents
  • Hi Venkataramanan,

    I think you could be OK to apply the input signal to the RF2 port (instead of RF1).
    Please note, when in OFF mode, RF1 is reflective open. Figure 1 needs to be corrected.

    We have not validated the switch for such application. The maximum power handling may be lower if input is applied to the RF2 port.

    Thanks,
    HK

Reply
  • Hi Venkataramanan,

    I think you could be OK to apply the input signal to the RF2 port (instead of RF1).
    Please note, when in OFF mode, RF1 is reflective open. Figure 1 needs to be corrected.

    We have not validated the switch for such application. The maximum power handling may be lower if input is applied to the RF2 port.

    Thanks,
    HK

Children
No Data