About ADI low phase noise RF amplifier

Hi, All

Just found that ADI has a new catalog : low phase noise amplifier as below pic.

But when I checked the datasheet of some amplifiers in the table, datasheet do not update the residual phase noise information.

I'm looking for a low residual phase noise amplifier which can amplify the output of a high performance OCXO/VCXO oscillator whose frequency down to 100Mhz.

I think the ADL5602 or HMC311 is good choice.

But I do not see related information in the datasheet of HMC311/ADL5602.

So ADI could provide the detail residual phase noise cure of HMC311/ADL5602 at 100Mhz?

Thanks a lot!

  

Parents
  • +1
    •  Analog Employees 
    on Mar 27, 2020 6:46 PM over 1 year ago

    Here are residual phase noise plots for HMC311 and ADL5602. In both cases the data was taken at 2 GHz. The file titles list the input and output power. We do not have data at 100 MHz but I would expect it to be better than this.  We are in the process of updating all of the datasheet in the above table, adding information on their residual phase noise.

Reply
  • +1
    •  Analog Employees 
    on Mar 27, 2020 6:46 PM over 1 year ago

    Here are residual phase noise plots for HMC311 and ADL5602. In both cases the data was taken at 2 GHz. The file titles list the input and output power. We do not have data at 100 MHz but I would expect it to be better than this.  We are in the process of updating all of the datasheet in the above table, adding information on their residual phase noise.

Children
No Data