Post Go back to editing

ADF5901+ADF4159

Hello,

I am using the ADF5901+ADF4159 chip combination to generate an FMCW ramp from 24GHz to 24.25GHz. However, the voltage on the VTUNE pin is always zero. I've been debugging the chips to figure out the problem. I have some questions in this context.

1. With the Vtune voltage at 0, will there be a spike in the current consumption in the ADF5901 chip, when the PUP Tx1 and PUP LO bits in register 0 are set to 1? If there is no spike in the current consumption, is it safe to assume that the VCO chip is broken?

2. How do we decide the BW and phase margin for the loop filter? My PFD frequency is 40MHz (REFIn:40M) and the required FMCW bandwidth is around 240MHz. I am using a loop filter designed earlier by my colleague. I am not familiar with loop filters. I've entered the filter components in the ADIsimPLL software and noticed that the BW and phase margin was 340KHz and 350deg respectively. Is this design correct?

3. If there is no feedback signal coming from the VCO (AUX and ~AUX), can the PLL still generate the ramp voltage if all the registers are set properly?

Thank you.

Best

Prateek



changed BW value
[edited by: prateekn at 11:29 PM (GMT 0) on 26 Feb 2020]