Post Go back to editing

initialize RFout ADF5901

`After powering up the device, administer the following programming sequence. The following sequence locks the VCO to 24.125 GHz with a 100 MHz reference and a 50 MHz reference divider frequency`

For the 5901 to operate at the full bandwidth starting from 24 GHz to 24.250 GHz, what should be the RFout be set to?