HMC641ALC4 P1dB

Hello!
What maximum power can be applied to the input of the HMC641ALC4 in the working frequency band 1kHz-70MHz?
What is the value of P1dB at 1kHz-70MHz?

  • +1
    •  Analog Employees 
    on Feb 13, 2020 8:11 PM

    Hi,

    HMC641ALC4 degrades power handling at frequencies below ~250MHz. HMC641ALC4 was measured down to 10 MHz where input P1dB is 15dBm. HMC641ALC4 could handle input power ~1dB higher (16dBm at 10MHz) than measured P1dB. 

    We don't have any test data for HMC641ALC4 below 10 MHz.

    Best.