Hello!
What maximum power can be applied to the input of the HMC347ALP3E in the working frequency band 1kHz-70MHz?
What is the value of P1dB at 1kHz-70MHz?
HMC347ALP3E
Production
The HMC347ALP3E is a broadband
high isolation non-reflective GaAs pHEMT SPDT
switch in low cost leadless QFN surface mount plastic
package. Covering DC...
Datasheet
HMC347ALP3E on Analog.com
Hello!
What maximum power can be applied to the input of the HMC347ALP3E in the working frequency band 1kHz-70MHz?
What is the value of P1dB at 1kHz-70MHz?
Hi,
HMC347ALP3E had been measured down to 100 MHz for power compression performance. HMC347ALP3E like other GaAs switches will start degrading power compression/handling below ~200 MHz. Based on test data of similar products, HMC347ALP3E would degrade power compression/handling by ~10dB at 10MHz compared to GHz frequency range.
Best.
Hi,
HMC347ALP3E had been measured down to 100 MHz for power compression performance. HMC347ALP3E like other GaAs switches will start degrading power compression/handling below ~200 MHz. Based on test data of similar products, HMC347ALP3E would degrade power compression/handling by ~10dB at 10MHz compared to GHz frequency range.
Best.