Hello.
Can I use HMC1118 for signal that have bandwidth 1 kHz - 10 GHz? Is HMC1118 able to work with signal frequencies below 10 MHz?
What is the value of P1dB at 1kHz-70MHz?
Hello.
Can I use HMC1118 for signal that have bandwidth 1 kHz - 10 GHz? Is HMC1118 able to work with signal frequencies below 10 MHz?
What is the value of P1dB at 1kHz-70MHz?
Hi,
HMC1118 is tested and specified to 9 kHz. However it could be operated at lower frequencies. The performances at 1KHz could be expected to be similar to 9 kHz.
Best.