ADAR1000 POWER INPUT

Hello,

I was wondering that what is the power values as minimum and maximum in transmit mode in ADAR1000 at  RF_IO pin? 

Also what is the receiver input ports's minimum and maximum power values in ADAR1000? Can you help me with this issues?

Thank you.

Parents
  • +1
    •  Analog Employees 
    on Dec 5, 2019 4:36 PM

    Absolute maximum ratings are found in Table 3 in the datasheet.  Maximum RF input power is 20 dBm, which would be the RF_IO pin in transmit mode, and each RX input in receive mode. 

    P1dB and Psat values are much lower for each path.  Please see Figures 22 & 23 for the receive channels, and Figures, 41, 42, 46 and 49 for the transmit channels.

Reply
  • +1
    •  Analog Employees 
    on Dec 5, 2019 4:36 PM

    Absolute maximum ratings are found in Table 3 in the datasheet.  Maximum RF input power is 20 dBm, which would be the RF_IO pin in transmit mode, and each RX input in receive mode. 

    P1dB and Psat values are much lower for each path.  Please see Figures 22 & 23 for the receive channels, and Figures, 41, 42, 46 and 49 for the transmit channels.

Children