hallo. Intrested use power detector out ,pin11. Register 0x03, bit6 . To on detector this bit 0 are 1? By reset it 1. but on pin11 present 1.5 voltage and no changes by rf signal. Is it open collector out ? BR
Hi,
Bit 1 will turn on the detector. Depending on the RF input you will have to change the DET_PROG bits in reg 0x07 (bits 0:6) to notice a change based on the RF power input. Note the ranges presented in the SPI map are based of the power input to the detector and not the RF input into the part so you will have to refer to the OUTPUT DETECTOR PERFORMANCE section as well.
Are you using a CW signal?
Thanks,
Hi
Is Voltage have presents on det out without rf power?
On pdf bit 0x3,6 shown as 0 (page 24)
"OUTPUT DETECTOR PERFORMANCE
Register 0x03, Bit 6 = 0, Register 0x03, Bits[13:12] set to 11, and TA = 25°C, unless otherwise noted"
is it error in pdf?
Hallo, Please check picture SPI load. admv no switch to BB mode
Pictured first 0B register loading
Pls provide a picture with the SPI lines labelled. I think I was able to deduce that one line is SCLK and another line was SDI but I do not know which one was SEN. If any of the other 2 lines that go low are SEN then I do not see it coming back up after the end of the SPI transaction. The SEN needs to come back up at the end of the SPI transaction to shift the data in.
How do you verify that part switches to BB mode?
Hallo
SPI send
{ 0x0B, 0x727C }, //VVA TEMP COMP { 0x03, 0x3857}, // DET EN BB3857 IF3157 { 0x04, 0x570A }, // 5.4 - 8 LO { 0x07, 0xD802 }, // Det out -14 +2 dBm { 0x0A, 0x2391 },
Pictured
after CS gous low 1,25 mS to clock
here pictured { 0x03, 0x3857}, // DET EN BB3857 IF3157
Do spi format is correct ?
admv1014 after power up in IF mode, and not set BB mode, RF signal outs by IF pins.
BR
here is reading data
0x00
0x01
0x03
0x04
0x07
Thank you for providing the labelled SPI waveforms. I think the SPI is working correctly.
In the write sequence could you add these 3 transactions?
1) Toggle the RST pin (high, low, high)
2) Write 0x4093 to reg 0x00 (soft reset)
3) Write 0x0093 to reg 0x00 (making sure soft reset bit is clear, if you're using parity bit then write 0x8093 but then this bit has to be cleared when writing to reg 0x0B).
Then complete the write sequence as you have shown above.
What are the power levels from the IF ports and BB ports when the part is in IF mode and BB mode?
When making these measurements please ensure that the VVA voltage is the same.
Also pls 50 ohm terminate the unused ports when making these measurements.
And let me know the RF and LO frequency that you are using so I can replicate it.
Thanks
Hallo . Power level presents only on IF out, no swich to BB.
VVA connected to 1.8V
VCTRL to ground
all unused port terminated 50 ohm
LO is 6 GHz, RF 36GHz
Please send you dev board SPI log
The ADMV1014 does not operate when BB or IF>6 GHz. With LO of 6GHz and RF of 36GHz the BB/IF frequency is 12GHz.
I took the data at RF=26GHz @ -30dBm, and LO=6GHz @ 0dBm (diiferential).
Here is the power out from an IF pin and the power out from IQ pin (there is no hybrid/ ac cap) installed. This is the direct power out from the pin.
-28 dBm-> IF pin, IF mode
-54 dBm-> IQ pin, IF mode.
-59 dBm-> IF pin , IQ mode
-33 dBm-> IQ pin, IQ mode
Also attached the simplified SPI log.
-- Analog Devices, Inc. evaluation macro file ## Copyright (c) 2019 Analog Devices, Inc. All Rights Reserved. This software is proprietary to Analog Devices, ##Inc. and its licensors. ## These code snippets are provided ‘as is’ with no warranties, guarantees of suitability, or acceptance of any ## ## liability, for their use. UI.SelectTab(Root::); Hardware.UI.AddAttachedHardware(()); > @Subsystem_2.ADMV1014-045188 RevA: @Reset(); [skip] >> @Subsystem_2.ADMV1014-045188 RevA.ADMV1014: @Reset(); [skip] >>> @Subsystem_2.ADMV1014-045188 RevA.ADMV1014: Evaluation.Control.WriteRegister(0x0, 0x4093); >>> @Subsystem_2.ADMV1014-045188 RevA.ADMV1014: Evaluation.Control.WriteRegister(0x0, 0x08093); >>> @Subsystem_2.ADMV1014-045188 RevA.ADMV1014: Evaluation.Control.WriteRegister(0x7, 0x0D808); >>> @Subsystem_2.ADMV1014-045188 RevA.ADMV1014: Evaluation.Control.WriteRegister(0xA, 0x2391); >>> @Subsystem_2.ADMV1014-045188 RevA.ADMV1014: Evaluation.Control.WriteRegister(0x0, 0x0093); >>> @Subsystem_2.ADMV1014-045188 RevA.ADMV1014: Evaluation.Control.WriteRegister(0xB, 0x727C); >>> @Subsystem_2.ADMV1014-045188 RevA.ADMV1014: Evaluation.Control.WriteRegister(0x0, 0x08093); UI.NavigateToPath(Root::System); @Subsystem_2.ADMV1014-045188 RevA: @DefaultView(); > @Subsystem_2.ADMV1014-045188 RevA: UI.NavigateToPath(Root::System.Subsystem_2.ADMV1014-045188 RevA); [ UI.SelectTab(tool.macrorecorder); UI.SelectTab(Root::System.Subsystem_2.ADMV1014-045188 RevA); @Subsystem_2.ADMV1014-045188 RevA.AD5601: Evaluation.Control.SetDecimalParameter(virtual-parameter-VCTRL_Voltage, 0, -1); @Subsystem_2.ADMV1014-045188 RevA: @Wizard(); > @Subsystem_2.ADMV1014-045188 RevA.AD5601: @ApplySettings(); [skip] >> @Subsystem_2.ADMV1014-045188 RevA.AD5601: Evaluation.Control.WriteRegisterMap(All, False, (), All, -1, False); [skip] UI.SelectTab(tool.macrorecorder); UI.SelectTab(Root::System.Subsystem_2.ADMV1014-045188 RevA); @Subsystem_2.ADMV1014-045188 RevA.ADMV1014: UI.NavigateToPath(Root::System.Subsystem_2.ADMV1014-045188 RevA.ADMV1014); @Subsystem_2.ADMV1014-045188 RevA.ADMV1014: Evaluation.Control.SetBoolParameter(RegMap1.Enable.IF_AMP_PD, True, -1); @Subsystem_2.ADMV1014-045188 RevA.ADMV1014: Evaluation.Control.SetBoolParameter(RegMap1.Enable.BB_AMP_PD, False, -1); @Subsystem_2.ADMV1014-045188 RevA.ADMV1014: @ApplySettings(); > @Subsystem_2.ADMV1014-045188 RevA.ADMV1014: Evaluation.Control.WriteRegisterMap(All, False, (), All, -1, False); [skip] >> @Subsystem_2.ADMV1014-045188 RevA.ADMV1014: Evaluation.Control.WriteRegister(0x3, 0x3857); [skip]
One clarification, this is the direct power out from the IF/BB pin on the ADMV1014 Eval Board. All the powers listed were not deembedded for cable loss and eval board trace loss. The purpose was to show that there is power output from the BB pins when switched to BB mode.