Hello.
I want to amplify voltage of few-ns-width pulse signal to ~100 V.
When I input pulse to HMC7748, would it work?
if it did, were there any way to calculate to estimated maximum output voltage and gain of pulse signal?
Regards,
SeeWoo Lee
When you say that you want to amplify a pulse, to you mean a short RF burst or do you mean a voltage that is zero and they jumps up to, say, 1V for a few ns and then returns to 0V. I think that you mean the second type of signal. I think that the internal ac-coupling of the module would mess things up. These devices are really designed to accept RF signals. So I would not recommend this device.