[HMC8205BF10] 10 ns-width pulse input and output?

Hello. 

I want to get output Voltage larger than 100 V peak to peak.

So I have some questions in the data sheet from figure 25.

< Output Power (POUT), Gain vs input power at 1 GHz >

for example, when 

Input: 24 dBm / Gain: 21 dB / output: 45 dBm    

 mean 

Input: (~3.5 Vrms) = (~10 Vpp)   /  output: (~40 Vrms) = (~110 Vpp)   right?? 

Then what would outcome be when I input 10 V-10 ns widh pulse to "HMC8205BF10" ?

How can I calculate the out voltage?  

and the pulse width of outcome would be similar to input? 

Regards,

SeeWoo Lee 

Parents Reply Children
No Data