[HMC8205BF10] 10 ns-width pulse input and output?

Hello. 

I want to get output Voltage larger than 100 V peak to peak.

So I have some questions in the data sheet from figure 25.

< Output Power (POUT), Gain vs input power at 1 GHz >

for example, when 

Input: 24 dBm / Gain: 21 dB / output: 45 dBm    

 mean 

Input: (~3.5 Vrms) = (~10 Vpp)   /  output: (~40 Vrms) = (~110 Vpp)   right?? 

Then what would outcome be when I input 10 V-10 ns widh pulse to "HMC8205BF10" ?

How can I calculate the out voltage?  

and the pulse width of outcome would be similar to input? 

Regards,

SeeWoo Lee 

Parents Reply
  • +1
    •  Analog Employees 
    on Oct 22, 2019 12:51 PM over 1 year ago in reply to LSW

    Hi SeeWoo,

                        I've attached a table of power levels and their corresponding voltages. This table is with respect to a 50 ohm characteristic impedance.  The HMC8205B is an RF power amplifier and we normally talk about its input and out put levels in terms of power and not voltage.

    PDF

    Regards,

    Jim B

Children