I Need application circuit and recommend component list of HMC789ST89E , ADL5320 for 950-1250 MHz band.
ADL5320
Recommended for New Designs
The ADL5320 incorporates a dynamically adjustable biasing circuit that allows for the customization of OIP3 and P1dB performance from 3.3 V to 5 V without...
ADL5320 on Analog.com
I Need application circuit and recommend component list of HMC789ST89E , ADL5320 for 950-1250 MHz band.
Hi Abdul,
I do not have an application circuit for the requested frequency range. I will need approximately 3 weeks to develop this circuit.
Regards,
Jim B
Thank you so much for you reply.
Dear can you please develop the application circuit and recommended component list for requested frequency range. If you can develop it as soon as possible it will be very effective.
Looking for your response.
Best Regards:)
Dear i also need you help for HMC1099LPSDE GAn amplifier IC. Can i use it at maximum 1250Mhz frequency because according to datasheet its frequency range up to 1.1GHz. However i did check the graphs of this amplifier and it looks like it will work fine at my frequency range which is upto 1250MHz frequency. Also can you please recommend me a biasing circuit for HMC1099LPSDE. It will be very helpful. You have been so helpful until now so i wanted to know your opinion on this too.Looking for your response.
Best Regards:)
Hi Abdul,
- Since ADL5320 is good enough for you, does this mean you do not need HMC789 tuning?
- when you say biasing circuit for HMC1099LPSDE, do you mean matching circuit or biasing?
if you mean biasing, that can be seen at page 14 in datahsheets.
Keep in mind that this is last time buy part, but you can use HMC1099PM5E instead.
Regards
Ivan
Sorry dear the part number was HMC1099LP5DE GAN amplifier.Actually i was saying about biasing circuit gate supply and drain supply voltages providing circuit.
Also i just see page 14 on datasheet matching circuit is provided. But i am talking about biasing circuit. Looking for your response.
Dear if you can provide me HMC789 application circuit i also add this device to my order list.Again thank you so much for your cooperation.
Hi Abdul,
Attached is the information about the evaluation board material and thickness.
Regards,
Jim B
Dear just looking for your response. Dear I also need application circuit of HMC1099LP5DE for 950-1250MHz frequency band. If you can help me it will be very thank full . Best regards:)
Dear just looking for your response ?
Hi Abdul,
I sent you email on 10/31 but I did not get any response.
Did you get that email?
Regards
Ivan
Hi Ivan Yes dear i received your email on 10/31 of application circuit and i also told you i just add this device to my order list .Actually i ordered the device. Now i required your help regarding application circuit of HMC1099LP5DE for 950-1250MHz. Dear i also need your prompt response. Best Regards:) Abdul
Hi Ivan Yes dear i received your email on 10/31 of application circuit and i also told you i just add this device to my order list .Actually i ordered the device. Now i required your help regarding application circuit of HMC1099LP5DE for 950-1250MHz. Dear i also need your prompt response. Best Regards:) Abdul
Hi Abdul,
You have not replied to that email, at least I have not received it.
Please reply.
Regards
Ivan
Dear i replied you here. You also want to reply by email ?
Hello Dear that was the reply i sent you on 10/31 in the reply of your email. I replied you here not by email.
Dear i also need your help for HMC1099LP5DE GAN amplifier IC. Can i use it at maximum 1250Mhz frequency because according to datasheet its frequency range up to 1.1GHz. However i did check the graphs of this amplifier and it looks like it will work fine at my frequency range which is upto 1250MHz frequency. Also can you please recommend me a biasing circuit and application circuit for HMC1099LP5DE at 950-1250Mhz band. It will be very helpful. You have been so helpful until now so i wanted to know your opinion on this too.Looking for your response.
Best Regards:)