I Need application circuit and recommend component list of HMC789ST89E , ADL5320 for 950-1250 MHz band.
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADL5320
Recommended for New Designs
The ADL5320 incorporates a dynamically adjustable biasing circuit that allows for the customization of OIP3 and P1dB performance from 3.3 V to 5 V without...
Datasheet
ADL5320 on Analog.com
I Need application circuit and recommend component list of HMC789ST89E , ADL5320 for 950-1250 MHz band.
Hi Abdul,
I do not have an application circuit for the requested frequency range. I will need approximately 3 weeks to develop this circuit.
Regards,
Jim B
Thank you so much for you reply.
Dear can you please develop the application circuit and recommended component list for requested frequency range. If you can develop it as soon as possible it will be very effective.
Looking for your response.
Best Regards:)
Following are the parameter for HMC789 :
Gain: 18-20 dB
P1db: +25 dB
IP3: +42 dBm
RL: 20 dB
NF : 3.8 dB
Hi Abdul,
What are your target specs for the ADL5320?
Regards,
Jim B
Dear same specs gain could be 20-21db with same frequency band as mentioned above.
Dear gain flatness should be as less as possible.
Thanks:)
- Is this input or output RL?
- Do you have room to lower specs, some trade off, for example Gain P1dB?
Regards
Ivan
This is output return loss.
Input return loss is 12db.
Dear these specs are the same as you given in the datasheet for other bands.
P1db shoulb be 25 db.
Gain can be 1,2 db lower as i mentioned above.
Thanks:)
houlb be 25 db.
Hi Abdul,
Can you tell us about more details about opportunity? What is company name doing this design?
Reason I am asking is because we might be able to find other part fitting your design target.
Thanks
Ivan
Our company name is aksa-sds. Aksa-sds is a design house providing engineering solution.
Hi Abdul,
I've been working the ADL5320 matching for 950 MHz - to 1250 MHz. Based on available load pull data the achievable gain in this frequency rang is about 16 to 17 dB? Before I go further and build a physical board will this amount of gain be adequate for your requirements?
Regards,
Jim
Dear thank you so much for your efforts.I think if you get 17dB gain it will be okay.Kindly proceed for further procedure.
Hello dear are working on the application circuit ?
Hello dear are working on the application circuit ?
Hi Abdul,
I have a circuit designed for the ADL5320. I just received eval boards so I can implement the designed circuit and verify the performance.
Okay dear thanks for your response.After verification share the results with me.
Best regards:)
Hi Abdul,
Attached are the results and the matching circuit. Gain is 16 dB. There is a trade off between IP3, gain and P1dB. I chose to maximize gain & P1dB. The matching components and location of components on th
PDFe EVB are in the document also.
Hi Jim,
Hi Jim,
Hi Jim , Thank you so much for your prompt response and helping i am really impressed. I just added the ADL5320 device to my order list. Your efforts and results are amazing. Dear just one more thing i want to know which material sheet and thickness you used for eval board.
Dear i also need you help for HMC1099LPSDE GAn amplifier IC. Can i use it at maximum 1250Mhz frequency because according to datasheet its frequency range up to 1.1GHz. However i did check the graphs of this amplifier and it looks like it will work fine at my frequency range which is upto 1250MHz frequency. Also can you please recommend me a biasing circuit for HMC1099LPSDE. It will be very helpful. You have been so helpful until now so i wanted to know your opinion on this too.Looking for your response.
Best Regards:)
Hi Abdul,
- Since ADL5320 is good enough for you, does this mean you do not need HMC789 tuning?
- when you say biasing circuit for HMC1099LPSDE, do you mean matching circuit or biasing?
if you mean biasing, that can be seen at page 14 in datahsheets.
Keep in mind that this is last time buy part, but you can use HMC1099PM5E instead.
Regards
Ivan
Sorry dear the part number was HMC1099LP5DE GAN amplifier.Actually i was saying about biasing circuit gate supply and drain supply voltages providing circuit.
Also i just see page 14 on datasheet matching circuit is provided. But i am talking about biasing circuit. Looking for your response.