ADRF5026, ADRF5044 Control Signal Application Relative to Vdd

For part numbers ADRF5026 and ADRF5044, I may not be able to control the timing of when control signals inputs get applied relative to the application of Vdd as described in their datasheets.

I understand if I apply a logic high to the switch control input without Vdd present, this can forward bias the protection diode and potentially damage.

I plan to have a 100 ohm resistor in series with each control signal input and 1000 ohm resistor in series with Vdd which would effectively limit current if/when this situation occurs.

What is a safe level of current that and flow through the protection diodes without damage? 

Thanks,
John