Hello,
I want to use RF switch HMC536 and RF attenuators HMC802, HMC629 for broadband application (LF...C-band). There is a requirement to use appropriate DC blocking capacitor in the datasheet on the RF input/output. Let assume that these parts are cascaded directly. My question is, if the internal DC pre-bias of RF pins is identical or very similar. Thus the DC decoupling capacitors can be omitted, RF pins routed directly and the RF performance is expected to be a better. Or is there any note about the DC voltage on RF pins in the datasheet?
Hi,
RF pins of HMC802A and HMC629A are dc biased Vdd. HMC536 has no supply input so its RF pins are dc biased by high voltage applied to one of the control pins.
If supply voltage of HMC802A and HMC629A…
It seems to me, if I compare AD similar datasheets (e.g.HMC470A), that the RF input/output pins are connected to the Vdd. Is it also valid for all mentioned P/N above?