Do you have gain and P1dB data for the HMC635LC4 at 85C? Would the part work at 90C?
HMC635LC4
Production
The HMC635LC4 is a GaAs PHEMT MMIC Driver
Amplifier die which operates between 18 and 40
GHz. The amplifier provides 18.5 dB of gain, +27
dBm Output IP3...
Datasheet
HMC635LC4 on Analog.com
Do you have gain and P1dB data for the HMC635LC4 at 85C? Would the part work at 90C?
Hi,
if this part is used even at 85deg life span will be shorten.
One solution is reducing Vdd from 5V to 4V.
Check P1dB and Gain at Vdd=5V over temp below:
Regards
Ivan S
Hi,
if this part is used even at 85deg life span will be shorten.
One solution is reducing Vdd from 5V to 4V.
Check P1dB and Gain at Vdd=5V over temp below:
Regards
Ivan S