ADAR1000 EVALZ General Questions

Hello,

I have some general questions regarding ADAR100 EVALZ:

1. There is a  J1 and J2 connector  on the board. But there is no description about this connection in the data sheet...

     In the data sheet there is only J5 described....and this line is not on the board..

2. Is the Technology of ADAR a CW or pulsed signal?

3. Is it possible to use TX/RX at the same time? Or do you have to use only TX for example and terminate the RX channels? In this case I can use a horn antenna for a RX...

I would be very glad, if you can answer these questions.

Thanks in Advance...