hi... i am using adf4351 evalution board, how can i make the bandwidth to 0 , and RF to 0 . please suggest me . what is the bandwidth in this case ? how to set the desired bandwidth
thanks,
balapavi
ADF4351
Recommended for New Designs
The ADF4351 allows implementation of fractional-N or integer-N
phase-locked loop (PLL) frequency synthesizers when used with
an external loop filter and...
Datasheet
ADF4351 on Analog.com
hi... i am using adf4351 evalution board, how can i make the bandwidth to 0 , and RF to 0 . please suggest me . what is the bandwidth in this case ? how to set the desired bandwidth
thanks,
balapavi
Hi Balapavi,
I could not understand your request. Could you explain in more detail please? Thanks.
Kudret
hi ... i am using ADF4351 ... I want to generate RF output as a 0 as well as bandwidth also 0 .. how to do this ?
see the below pic ... red mark is bandwidth frequency right ,,,
Do you mean "0 dBm output power" or "no output" by saying "RF output as 0"?
The marked settings are for the VCO band selection timing. What is the requirement of your application?
What is the bandwidth that you are referring to?
yes ,,actual i need generate a pulse signal , on and off . on for 40msec milisecond and off for 100 milisecond . this is thing i need to do .. and then power should be 100-300 mW
then how to make 0 dbm is it possible ?
Thanks,
balapavi
can we able to program this board, mean debugging my own code to this .. which software i could use
Hi Balapavi,
Minimum output frequency for ADF4351 is 35 MHz with %50 duty cycle. It is not the right part for your application. Your application requires a timer. You can check TimerBlox products from below link.
https://www.analog.com/en/parametricsearch/11410#/
I think what you need can be done by using LTC6991. You can use TimerBlox tool from the following link.
http://beta-tools.analog.com/timerblox
I created an example using TimerBlox tool as below. You can change the values according to your requirements.
Regards,
Kudret