ADMV1014 reserved register values

Hello.

The ADMV1014 has a number of bit fields which the datasheet says are read only.  For instance bits 15:10 and 5:4 of register 0x4:

If I write to these "read only" reserved bits and then do a read back, the reserved bits have change to the value I wrote, suggesting that these fields are actually read/write.

For instance, If I write 0x7FF8 to register 0x4 and then do a read back, I get 0x7FF8.  Clearly reserved bits 15:10 have changed to 0b011111 which should not happen if these bits are truly read only.

Can Analog confirm whether this is the expected behavior?  Even though they are changing, does the device ignore the reserved values, or do I need to set them to the datasheet values?

Thanks for the help

Parents
  • +1
    •  Analog Employees 
    on Aug 22, 2019 6:33 PM over 1 year ago

    Hi,

    These are reserved bits and not read only bits. Some of them are used for internal debug purposes and not meant to be changed. Changing these bits could potentially affect part's performance. The datasheet has them shown as read only as we don't recommend writing and changing the values.

    Some of the other reserved bits are not connected to anything, however we still do not recommend changing them.

    Thanks,

Reply
  • +1
    •  Analog Employees 
    on Aug 22, 2019 6:33 PM over 1 year ago

    Hi,

    These are reserved bits and not read only bits. Some of them are used for internal debug purposes and not meant to be changed. Changing these bits could potentially affect part's performance. The datasheet has them shown as read only as we don't recommend writing and changing the values.

    Some of the other reserved bits are not connected to anything, however we still do not recommend changing them.

    Thanks,

Children