ADAR1000 EVALZ -some questions about the software

Dear,

When I use software,Operating as follows:

Take the receive channel

Put through power supply,+3.3V and -5V 

1、 ,click the connect

2、 ,The operation is shown in the figure,and click the write

3、 The operation is shown in the figure,and click the write,The current is 30mA

4、 ,The operation is shown in the figure,then ,click the LDRX OVR,the current is 70 mA,Shouldn't it be 230mA?

When I click the start, ,the current is 230mA,WHY??

I also want to know ,What is the relationship between rx control and RX registers,One is register control,and the other is?Whether they work simultaneously or separately