How to use ADL5910 peak/envelope eval board to get peak voltages with peak period 1.67 seconds

hi there,

i have bought an ADL5910 peak/envelope eval board to get peak voltages with peak period 1.67 seconds.

basically, the element i am trying to measure has a peak voltage of around 0.4 to 40 volts which occurs every 1.67 seconds.  All I want to do is get the peak voltage from each pulse and output those values to a microprocessor.  

I have been trying to use the data sheet which describes the 5910 but it doesn't seem to indicate where to measure the output - I tried Q but it seems this is just the flip-flop as it outputs 0 or 1 only.  If i'm running the signal into Rfin_SW, do I measure output peak values at Rfout_SW?  Also, it seems that the board has to be reset manually from outside after each peak is detected - is that right?

Any help much appreciated as, clearly, I am a newbie on this stuff.

Cheers, Nick

Parents Reply Children
  • 0
    •  Analog Employees 
    on Jun 14, 2019 11:56 PM in reply to boydy33

    Hello boydy33,

    • Is there a RF carrier frequency for your “…spike/pulse of every 1.67 second in signal...” ? You need an input RF signal from the tenth of kHz to 6GHz.  The ADL5910’s TCAL (or VCAL ) pin has a typical output voltage at about 750mV with no RF Input    You measured 765mV indicating that the input signal is too low or your input signal could not get to the ADL5910 device.
    • You do not need external voltage supplying to the Vin pin.  You can adjust R8 potentiometer for it.
    • When the ADL5910 is latched, the Q output will stay on “High” .  At the same time, the RST pin is pulling low (by R5 resistor).  The ADL5910 will stay at latched condition until the S1 switch is pressed or a voltage that  greater than 2V that supplying to RST pin.
    • The signal at  RFOUT_SW is from the RFIN_SW input signal.  When the ADL5910 is latched, the Q output is  “High”.  The "Q_bar" is "Low" and it will open the switch (HMC550A) which prevent the signal flowing to the RFOut_SW.

    Hope these can help.

    John_C

  • Hi John,

    Thanks a lot for your help on this man - much appreciated - as you can see, I' m a mechanical engineer, not electrical ;-)

    • Is there a RF carrier frequency for your “…spike/pulse of every 1.67 second in signal...” ? You need an input RF signal from the tenth of kHz to 6GHz.  The ADL5910’s TCAL (or VCAL ) pin has a typical output voltage at about 750mV with no RF Input    You measured 765mV indicating that the input signal is too low or your input signal could not get to the ADL5910 device.
      • The input I am measuring is an electric fence, which is energised by a normal electric fence energiser.  This charges an internal capacitor and discharges 2 to 12 kV down the fence every 1.67 seconds in the case of my fence.  Hence, I don’t believe there is any carrier signal between peaks. 
      • My assumption in all this is that this is the point in the calibration procedure where you need to connect your background noise signal to RFin but is it the case that you are actually applying your full signal with voltage pulses at this point  in the procedure?
      • Does your above comment mean that if there is zero voltage applied between voltage pulses, then this board cannot detect the pulses?  Isn’t is possible to trigger reading of the pulse peaks in this case just by setting the Vin to the effective zero level of the ADL5910 board– ie. 750 to 767mV?
      • If I can’t do it with this ADL5910, do you think this type of circuit would be more appropriate? https://web.archive.org/web/20160624...ul/peak_holder
    • You do not need external voltage supplying to the Vin pin.  You can adjust R8 potentiometer for it. 
      • I suspected that was the case…thanks.
    • When the ADL5910 is latched, the Q output will stay on “High” .  At the same time, the RST pin is pulling low (by R5 resistor).  The ADL5910 will stay at latched condition until the S1 switch is pressed or a voltage that  greater than 2V that supplying to RST pin.
      • Right, so I’d basically have to trigger the reset to S1 by applying a voltage of > 2V to the RST pin.  That shouldn’t be difficult to program and supply from my microcontroller.  Thanks.
    • The signal at  RFOUT_SW is from the RFIN_SW input signal.  When the ADL5910 is latched, the Q output is  “High”.  The "Q_bar" is "Low" and it will open the switch (HMC550A) which prevent the signal flowing to the RFOut_SW.
      • Sorry John but I’m a bit confused by this.  I still don’t understand where exactly you would read the output, peak, signal and what exactly it would be – ie. Digital or analog signal? So say, the max peak voltage found during a given pulse is 30 volts, where would you measure that and in what form will it be….I assume it would be an analog signal right?

    cheers,

    nick

  • 0
    •  Analog Employees 
    on Jun 19, 2019 4:01 PM in reply to boydy33

    Hello Nick,

    If you do not have input RF signal, the ADL5910 device will not work with your application. 

    John_C

  • Sorry John but I'm really not quite sure what you mean by not having an RF input signal?  I do have one, as described in previous posts including images in the early posts.  Perhaps I am confusing this with some other separate input signal?  Explanation much appreciated.  Cheers, Nick

  • 0
    •  Analog Employees 
    on Jun 22, 2019 12:20 AM in reply to boydy33

    Hi Nick,

    Reading through the above correspondence, it's not clear from your oscilloscope photo if there is an RF carrier wave present, or not. A much higher resolution photo is necessary. Offhand, so far, it looks to me like you would be better off with the diode and op-amp peak-detector circuit, like you posted the web link for, above. I might add that you can use our LTspice to help simulate the RC values to give favorable attack and decay times for the circuit that will work best with your MCU.