Hi all,
We have some questions about HMC1113.
1.Which Is the Lo drive input for each MIXER "0deg/0deg" or "0deg/90deg" ?
2.Is the IF output phase correct ?
・IF1(20PIN):0deg
・IF2(18PIN):-90deg
3.How to select the appropriate sideband ?
Following is correct ?
To select the lower sideband, connect the IF1 pin to the 90° port of the hybrid and the IF2 pin to the 0° port of the hybrid.
To select the upper sideband, connect the IF1 pin to the 0° port of the hybrid and the IF2 pin to the 90° port of the hybrid.
Best regards,
sss