Post Go back to editing

Question on Mixer for upconverting

Dear Analog Devices,

I plan to make the up-converting system with the freq. range as below.

IF : 500MHz ~ 1250MHz

LO : 2GHz

RF : 2.5GHz ~ 3.25GHz

Is there any evaluation board of mixer which can meet the requirement as above?

I've searched several mixers on your site, but it seemed that there is no evaluation board to cover the frequency that I've mentioned.

If there are no evaluation board, is there a way to design circuit to meet those requirements?

Thanks in advance.

Top Replies

Parents Reply Children